This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP8860-Q1: Connecting 10 RGB LEDs in series

Part Number: LP8860-Q1

Hello, Team,

Our customer is trying to use LP8860BQVFPRQ1 to control RGB LEDs which I_LED is 5 ~ 50mA.

Forward voltage Vf in case of forward current If = 20mA is as follows:
Red: 2.05V
Green: 2.60V
Blue: 2.85V

If we connect 10 LEDs in series, the Vf difference of Red and Blue would be 8V; Would there be an issue such as thermal problem of driver FET getting hot?

Best,
Masaru Oinaga