This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65051-Q1: LDO input and output

Part Number: TPS65051-Q1


Hello,

Backflow prevention of TPS65051 LDO.
When the power is turned off, the input voltage and output voltage of VLDO3 gradually decrease.
There is a Schottky diode between VLDO3 and VIN_LDO3, but it reverses the input and output voltages on the way down.
Is there any problem?

steady state
Input Voltage: 3.9V
Output voltage: 1.3V

in the middle of powering off
Input voltage: 190mV
Output voltage: 200mV

Best regards,

Akitoshi Mukaiguchi