This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR23630: External VOUT control method

Part Number: LMR23630

Hi team,

My customer is using LMR23630AFDDA to adjust output power with DAC.
Their boards are tested swinging DAC voltage.
When it is set to 1V output, some devices broken.
The failure mode is FB terminal shorted to GND.
If OP-amp sinks current from FB terminal, is FB terminal broken?

Best Regards,