This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD90320: Fault log function

Part Number: UCD90320


Hi 

It takes 45ms~55ms for UCD90320 to bootup when P3V3 is available.

But how about fault log function of it?

Is this function active when P3V3 availiable? Or do it still need 45ms~55ms?