When we have done a data collection run in order to generate an .aux file, we have noticed the cell 1 parameters have been significantly different compared with the other cells. Qmax is always lower and the Ra values differ. We suspect this is an artifact of the chip being powered from cell 1 and no balancing being allowed during data collection.
Do the differences in parameters have any detrimental effect on impedance, or other calculations?
Is there a solution to this problem other than to use the 'generic' setting when creating an .aux file?