This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5022-Q1: LM5022QDGSTQ1

Part Number: LM5022-Q1

Hello, 

We our trying to design a boost converter. 

Specification 

Vin min - 40V Vin max - 56V. 

Vout - 72V. 

Iout - 3.5A. 

Based on our requirements we used TI webench for designing.  

We designed the circuit & PCB as suggested by Webench. But the problem is the output voltage is same as that of input voltage. For e.g. @48V of input supply the output is also 48V. 

I am attaching the Webench design & our circuit schematic https://drive.google.com/file/d/12G2P0QTnLjonFxk91GwlJD6__s3S946Z/view?usp=sharing