Part Number: LM7310
Other Parts Discussed in Thread: TPS2663
Hello team,
I want to enable Charger after detecting battery ( battery insertion ) so that i can protect charger IC from In rush current and any instaneouse voltage fluctuation.
I will on the load switch using Host after battery inserted , untill it will remain OFF.
Battery Charge Current is 2A and Max Voltage is 18VDC.
Can I use LM7310 for same or you can recommend any best suited one ? Allocation diagram is as follow.