I need a boost converter controller of Vin_min. 2.5V to 3V and Vin_max=<7.5V (sync. or non synch), can able to produce of output 12V/10A.
Please suggest a controller
Thanks and Regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Joseph,
12V/10A means 120W. For an input voltage of 2.5V, this means something like 56A if the efficiency of the converter is at 85%. Is your source able to support such a high current?
I think you need to use several converters in parallel for such a high output power.
Have a look at this reference design for 100W: PMP10749 reference design | TI.com
Best regards,
Brigitte