Hi!
I designed a schematics and PCB for a charger. in which I used PFC and then phase shift full wave bridge rectifier. In this PCB, PFC is working perfectly but for the H-bridge I am using UCC27714 for controlling MOSFETs of h-bridge. when I have the VCC_PFC and PWM signals, I the VCC_PFC (which is 12V) is dropped to few mV while checking the short test do not give any short circuit in VCC_PFC and GND. as this same VCC_PFC is going to PFC and PFC work but when I connect the H-bridge board, PFC also stop working
Can you review and my design and give me suggestions?
While testing, I am not giving any power on P1. I am first checking the pulses on the gates of MOSFETs.5557.PCB_Project.pdf