Hello, I am trying to use the TPS2041D in order to limit the current for a USB 5V output to 500 mA per USB 2.0 specs. I am doing some typical and max power estimates for a PCB design in order to provide data for thermal analysis. Worst case would be to 85C. The datasheet states a continuous total power dissipation for various TA temperatures for the D package, and at T@ = 85C, the power dissipation is 377 mW. Is this considered max power? Could I get some advice on calculating typical and max power based on my application? If needed, I could provide a schematic snippet of the circuit. Thank yo for your time.