hi,
I am doing a design using UCC28951 following the recommended circuit similar to below:
my MAX load is 42A 12V. but when the load < 6A, the signal to OutB (pin21) and OutD (Pin19) with reference to GND will have unstable duty cycle at OUTB and OUTD. But the OUTA and OUTC is stable.
OUTA and OUTC output is having stable during cycle/ This is output CHA , blue is output from Pin 22 , Pink is form Pin 7 IC 2
However, OUT B and OUT D is having unstabel durty cycle
you can see from this waveform, the duty cycle is unstable.
Can you advice how can i get a stable duty cycle even at <6A load?