This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54302: Not Compatible with TPS54308?

Part Number: TPS54302
Other Parts Discussed in Thread: TPS54308

Hello E2E Experts,

Good day.

When the TPS54308 was unavailable, we substituted the TPS54302 with no other cct modifications. The application is 24VDC input, +/-3.3VDC output at 1A.

 Schematic:

Note: 22ufd Caps C106,107,112,113 PN is TDK C2012X6S0J226M series. C108 PN is TDK CGA6P3X7RIE226M250AB

The 302 device in cct produces the following positive output with ~200mA positive load and 0mA negative load:

The same cct with TPS54308 installed on the identical PCB, the same loads output is:

PCB Layout (top layer of 6) full ground plane in layer 2:

What am I doing wrong? Any help would be appreciated.

Regards,

CSC