This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65994AE: VBUS connection when using external power path as source

Part Number: TPS65994AE


Hello team,

Is it okay to connect internal source path (PP_5V) to VBUS when using the external power path (PP_EXT) as source, like on the picture below? Do I need load switch?

I am concerned that it might confuse the device because external power path is mean to be sink.

(I have confirmed that external power path can be configured as source)

Best Regards,

Kei Kuwahara