hello, tech support at TI:
i am seeking your recommendation on a vital signal to track the performance degradation for the rechargeable battery since we are using bq40z50-R2 as fuel gauge, here is a list of parameters i would like to track:
1) impedance tracking and
2) SOH measurements. (pack level)
3) QMAX parameter. (which is the max capacity in mAH) on a per-cell basis.
4) charge cycle count
the goal of the task to come up with a remaining useful life estimate model for predictive maintenance schedule based on the health monitor log file database.
i am seeking your recommendation to confirm if i capture all the critical parameters or some parameters in my list is not critical or if i miss any critical parameters to be captured in the fuel gauge ?
Thanks
jason