This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28065: UCC28065 on-time calculation

Expert 6760 points
Part Number: UCC28065


Do you have a formula to calculate the on-time, based on the value of Rtset and the voltages applied to the Vinac and Vcomp pins?

  • Hello Isee.

    Thank you for your interest in the UCC28065 PFC controller. We don't publish some of this information outside of TI, but I can reduce the formula to give you what you need. In order to accomplish this, I had to boil down some internal factors to a constant (0.7). This should get you very close.

    For example: Vcomp = 5V, Rtset = 66kΩ, Vinacpk = 0.6V: Ton ~ 143.6uS.

    Regards,

    Ray