Part Number: LMS3655
Dear TI team
I would like to use "LMS3655" under the condition of "24VIN/5VOUT".
Also, this time, I would like to add a 5V backup circuit using a supercapacitor to the output side of the IC.
(I checked the application note below.)
I have a question about turning off the power supply to the "LMS3655" and setting VIN to 0V.
At this time, if the supercapacitor is charged, "VIN < VOUT" may occur, and the current may flow backward through the parasitic diode.
Is this perception correct? Also, if there are any other possible problems, please let me know.
Also, I'm thinking of placing a diode for reverse current prevention at the position shown in the attached figure.
I realize that by putting a diode between the FB resistor and the inductor, I can keep the output voltage at 5V without worrying about the voltage drop due to the VF of the diode.
Is this perception correct? Please let me know if I've overlooked anything.
Best Regards,
Taroimo