Hi All,
TPS65983B is hardware-configurable to present Rd_DB (Dead Battery) during dead battery, when an external connection pulls up on C_CCn (the case when connected to a
pull-up resistance Rp or pull-up current), the connection through R_RPD will pull up on the FET gate turning on the pull-down through RD_DB.
My question is the FET gate could be continued turning on while the voltage on Sink CC Pins is 0.25V~0.61V (Default USB )?
Because the min VTH_DB of TPS65983B is 0.5V, I assume the FET will be turned off quickly while voltage on Sink CC Pins is below 0.5V.
BR,
Wilson