This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS22919: Switch-on timing are only typical values, we need maximum values

Part Number: TPS22919


In the datasheet, there are typical values for switching times only. Switch on time rises significantly at low temperatures. I understand that rise time would be dependend on many parameters. But from my view one needs a good estimation of maximum times. In our very simple design, where a battery is connected to a high impedance voltage divider, the switch on time seems to be largely dependend on temperature and differ from device to device. We use a 3.6V battery, a resistant load of 40kOhms and temperatures from -40°C to +85°C. Question: would be 3 milliseconds enough to ensure voltage rises to 98%?

  • Hi Wolfgang, 

    We do not provide maximum times for ton. After reviewing our characterization data across temperature, I would recommend waiting 5ms for the voltage to rise >98%. 

    Do note, this value is not guaranteed by TI as it is not in the datasheet. These values should serve as a design reference only. 

    Best Regards, 

    Elizabeth