This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Reg Battery Charging & discharging to Inverter

Other Parts Discussed in Thread: TPS5410

Hi all,

Micro-Inverter application.

i want to charge battery (12V or 24V) from solar PV input (25V - 55VDC). can anyone suggest me the stepdown ic for this application. whether i can use TPS5410/20/30.

And the battery output i need to give as an inverter input and to produce AC output (DC to AC) 110VAC / 220VAC with 200W. So for this can i go with boost / push-pull topology.  Kindly suggest me the Controller ic or any other better solution for this application.

 

Thanks 

Suresh

  • You have not provided enough information to select a power supply.  When you have narrowed down your electrical requirements, you can select an IC from the Power Management Search Tool found  on www.ti.com and then click on Power Management.

    For the inverter, if you are not a power supply expert, I will suggest that you work with a contractor company to design this supply.  TI has many ICs that will meet your requirements, but you will need to understand the power supply topologies you mention in order to properly use the ICs.