This datasheet ( www.ti.com/.../snosdg2a.pdf) contains contradictory information regarding which pin is pulled low when an overcurrent event happens. On Figure 8-5 there is an /OC signal and then in Figures 9-1 and 9-2, the ZVD pin is labeled with ZVD/OC. Based on these, I would assume that the ZVD pin is used to signal OC events. However, in 8.3.7.4 it is said that OC events will hold low the /FAULT pin, and the ZVD pin is not mentioned.
Can someone clarify which pin is used to signal an overcurrent event?