This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM74900-Q1: Load dump output discharge path

Part Number: LM74900-Q1

I am using LM74900Q1 on the input side of the module.

It receives battery power and connects it to the DCDC at the rear end. If LM74900Q1 is disabled in a UVLO or OVP situation,

I wonder if the discharge path of the output voltage is inside the chip.


If not, I think I need to attach resistance for the discharge passage,

but I'm asking how many ohms I should attach for the bleed resistance.
For reference, the output voltage is 9V to 16V and the current is at the peak 7.5A level.