Hi guys,
I'm looking into the BQ24725 battery charger and was wondering if I could choose to power the system from the battery even when the AC Adaptor is present. (not while charging)
From what I gather this is not directly possible from accessing control registers via the SMBUS. I see that we can disable the charging function - but the system will still be powered from the AC adapter as long as it is present. Is this correct?
If this is correct, can I assume that the only way to accomplish this task is by controlling the voltage on the ACDET pin? For example (Figure 2 BQ24725), could I add FET/RESISTER (in series) parallel to R2 such that when the FET is on, the voltage at ACDET is reduced and the battery is chosen to power the system instead of the AC (by fooling the chip into thinking the AC adaptor voltage is invalid). Is this a practical solution?
Are there a similar TI chargers that have this functionality?
Thanks