Hi team,
Thanks for your support always.
In this case LM5156-Q1 is supplied power to sensor that Vin = 12V to Vout = 18V. Since our customer system has a request need < 0.1mA when system is standby. If I disable sensor still have ~10mA Quiescent current at sensor. therefore customer would like to shut down the boost to meet the request.
As I know that boost can't disable directly because of it architecture [mosfet open(Duty = 0%) -> Vout = Vin]. Only way I can think is add switch at Vin/Vout to disconnect the power rail. Do you have any idea to let boost stop providing power?
BR,
Jimmy