This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS709: behavior without load

Expert 6760 points
Part Number: TPS709


Goal is to create 3.3V from 15V

If operated without load it only regulates up to a Vin of 9.7V the output correctly.

Beyond that the Vout increases according to Vin.

If the output load is 660 Ohm everything is fine.

Are there some minimum requirements I have overlooked?