I am using a TPS40200 to supply 27.2V @ 1.65A from a 37V input. When I increase the load to a point were over current protection circuit trips, the parts enters the "Hiccup" mode as described in the data sheet. The problem is when I remove the load the part still remains in "Hiccup" mode and cannot self recover. I need to remove the input power and let everything "drain down" and reset in order for the part to startup again and achieve proper regulation. When the part is in "Hiccup" mode the output is a very ripply 8V or so. What can I do to help the part self recover. How sensitive is the compensation network? And is it posible to vary the output voltage on the fly by pulling on the Feedback resistor divider?
Please help! :-)
Thanks.
Eric
Sr. EE at Medtronic in Littleton MA