This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A14: Facing issue with TPS7A14EVM-058 EVM

Part Number: TPS7A14

Hi Team,

As per the datasheet of TPS7A14, IQ(Bias) at Iout-1A is 12mA.

We have checked the same with TPS7A14EVM-058 EVM , in EVM VBias pin is taking 100mA from 3.7 supply (Vbias voltage) and we are not getting exact 1.3V at Vout.

we have provided 1.45V as input and our load will consume approximately 650mA.

Please clarify, why this Vbias pin is taking too much current? is this due to EVM issue?

Thanks & Regards,

Dharani. T