This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS22992: Vin specification

Part Number: TPS22992

Hallo team,

Is it acceptable to have no input on Vin when VBIAS and ON have 3.3V?

  • Hello, 

    Yes there is no concern with Vin being low with VBIAS and ON high. 

    Do note if the device is enabled, the device will output whatever voltage is on the input, so if Vin is floating, you will see whatever voltage on Vin, on Vout. 

    Best Regards, 

    Elizabeth