This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54360B: transient load limit

Part Number: TPS54360B
Other Parts Discussed in Thread: TPS54360

If we design a TPS54360B for 2.1A , 3.1Vload at peak, how can I make sure the buck will be stable if the load transience is at 10Khz from max to min on the load side.

Also the input voltage is 26-48V and the switch frequency is about 300Khz or same as the simulation that can seen on the work bench