Part Number: TPS25750
Hi,
I want to use the TPS25750D with a tablet (OUKITEL RT2) as source and sink. The tablet reports the capabilities SNK 5V@2A and SRC 5V@1.5A.
If the tablet is a source it works a expected. But if the tablet is a sink it only accepts 0.5A, although the register 0x34 ACTIVE_CONTRACT_PDO, shows that the 5V@3A profile is selected.
Is there a configuration that I need to change to allow a current of more than 0.5A?