Other Parts Discussed in Thread: SE555, LM555, NE555
hello,
I made a small prototype that implements the scheme shown in the figure below to convert an input 48Vdc (40Vin-60Vin) into 245Vdc for 65W of power.
As you can see, the LM5023 IC power supply is isolated from the primary 48Vdc power supply and the VSD pin is left floating.
I encountered the following problem. When I apply a short circuit on the output, the power mosfet continues to be driven with a short duration pulses, causing the mosfet to overheat very quickly.
Not being able to use the auxiliary winding to power the IC, how can I fix this?