Other Parts Discussed in Thread: BQ25792EVM
Dear TI E2E Team,
I am writing to report some issues I encountered while using the BQ25798EVM development board. Specifically, I have encountered the following three problems:
-
Despite following the 2.4 Test Procedure, the LED (D13) did not light up. Instead, when I installed the shunt in JP17, the LED (D13) turned on. Can you please explain why this is happening?
-
I followed the 2.4.2 Communication Verification steps and set the parameters (including VSYSMIN, Charge Current, IINDPM, etc.). However, during the 2.4.3 Charge Mode Verification, the measured VBAT and REG1Cb[7:5] did not match my expectations. What steps can I take to resolve this issue?
-
According to the specifications, the REG06_Input_Current_Limit Register should be set to 3000mA upon reset. However, no matter how many times I try to modify it, the IINDPM can only be measured at 1420mA or below. What can I do to fix this?
For your information, my PowerSupply is set at 5V and 3A. Load#1 is a DC electronic load set at 7.6V and 2A, while Load#2 is the only 50W 10-ohm cement resistor.
Thank you for your attention to these matters. I look forward to hearing from you soon.
Sincerely,
Freddie Jhneg