Other Parts Discussed in Thread: BQSTUDIO
hi
we are using BQ40Z80 in our Li-ion battery packs
we had several designs but the phenomena of Full charge capacity degregation we see in all the types,
the application is robotic and the robot is always working between 15%-85%, once in 50 cycles he goes to full charge and rest,
we see that after even 30 cycles the full charge capacity cuts to 70% and this affect on the work time
I attached .gg file for one of our batteries,
Are the known issues?
are there any issues that we don't do right?
is there any way to pix battery like that? any command or something?
maybe we can schedule with a TI expert on that issue?