Other Parts Discussed in Thread: LM5123-Q1, LM5156
Hi Team,
My customer is surveying boost converter IC to support 48V/5A output, 10V~16V input range, is LM5157 applicable for this power level?
Regards,
Charles
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Thanks for reaching out. The peak current limit of the LM5157 is only 7.5A typ, therefore this IC is not suitable for the specs above mentioned. Please consider using the LM5156 which is a controller or the LM5123-Q1 (which is a synch boost controller).
Kind regards,
EM