This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Boosting 24V to 90V 20A

Other Parts Discussed in Thread: LM5122, LM5170

Hello, i need help with part selection for making a boost converter that can take 24V DC and boost it to 90V. I need to supply 20A to the output. I have looked at the LM5122 and the LM5170, but the LM5170 only boosts to 85V. I was wondering if there was a controller that is like the LM5122 but has an easier capability to do more than 2-phase.