Hi, I'm using TPS54040 in one design, it worked on the rev1 board, but on the rev2 board, it doesn't work. Rev2 shares the same design, and PCB layout is same as well.
The design is to have 5V in, 4V out, 650KHz switching frequency, and input should also work with 12V input as well. I disconnected the load, measured output, found that output is similar to saw wave with around 8-9Hz change frequently from 2.7 to 3.6, and Pin 10(PH) output the similar wave, 8-9 Hz saw wave. Looks like internal oscillator is not working properly, I checked resistor connected to Pin5(RT), it's correct. I'm wondering is there any possibility could cause this problem.
Thanks.