Hello, I am currently trying to use this part to driver a power mostfet. I designed according to the datasheet. This is the output waveform. The problem I am running into is why is the output of the gate driver inverted? I am concerned this negative voltage will affect the power MOSFET I am attempting to drive. Attached are images of the application note and output of M1 being driven by a PWM source Rext ~ 290 ohms. Any tips/advice on gate driver implementation would be helpful.