Hi,
What is the maximum output current that can be delivered to the VO and VSNS pins of the IC.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Rohit R,
The sink current limit maximum here is 5.5A. Please also note that as output current goes down, the output voltage goes up. This can be seen in the 'Load Regulation' figures located in section 6.6 labeled 'Typical Characteristics' of the datasheet linked here.
Thanks,
Field