Other Parts Discussed in Thread: TL317, LM317
Hi expert,
can you provide the LM317L dropout curve VS current? the datasheet only tell me it is up to 2.5V.
Besides, can you provide a P2P device under TSSOP8 package? Input voltage is above 7V and less than 8V, output is 5V. current is 80mA, better to above 100mA.
I only find TL317 is p2p toLM317L and have better drop out.
so what is the max dropout for LM317. It only have 25C characters.
BR
Emma