Other Parts Discussed in Thread: TPS61193,
I have build the same circuit used in TPS61193/Q1 Evaluation Module in PSpice which is shown below to check model is working or not.
My PSpice simulation Circuit is shown below
Output waveform of PSpice simulation circuit
As you can see the I am getting 5V output which I have applied as input,
Enable pint voltage is 5V, But i am getting 499uV at fault pin, means TPS61193 is generating fault signal, Please help to solve debug the circuit,
Is anyone is siumlated the TPS61193-Q1 in PSpice so we can confirm the PSpice model is working properly.