This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM74722-Q1: Pspice simulation

Part Number: LM74722-Q1

Hello,

I am trying to simulate the ISO 7637-2 pulse 1.

Why Vin is fluctuating if i consider load as around 20A.

If i take load around 50mA, then Vin is not fluctuating.

What is the reason behind this problem.