Hi,
I'm looking for a device that is controlled with I2C that would give sixteen open drain MOSFET outputs where I can sink a small current into the output MOSFETS (30uA) via a resistor. The resistors are supplied by a constant current source, but at 24V. So I'd being going 24V -> High Side Constant Current Source -> Resistor -> Open Drain output of expander.
I have found several devices, but they all seem to have a low maximum output voltage. TLP9202 looks close, but is SPI. TPL7407LA looks like it would do if it was I2C controlled and have four address bits so I could have enough 8-bit devices on the board. So, I think the perfect device would be a sixteen bit TPL7407LA controlled by I2C.
I did look at LED drivers, but they are seem to have constant current drivers built into them and that's no good for this application. I suspect if there was an LED driver that was simply switching on and off, that would be cool.
Thanks!
Rob