This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR36006: Output rails to max value

Part Number: LMR36006


I've been trying to use the LMR36006 in a simple circuit to down-regulate from an input of 12V to ~6V, for a low power ion trap driver application. Despite my best attempts, the output will not appear to regulate itself and always rises up to nearly the input voltage, or ~11.8V. I'm running out of possible explanations and am hopeful someone can help me. The list of attempts I've already made are below.

  • The FB voltage produced by my circuit is ~1.97V in this condition, which should notionally signal the LMR36006 to stop switching and let the output settle. Initially I was concerned the IC FB pin wasn't soldered properly, but I no longer think this is true (probing the IC directly and not the underlying pad shows the 1.97V)
  • Adding a dummy load resistor to increase the output load current above a low standby current level has no noticeable effect, beyond the output falling a bit (presumably due to ohmic loss)
  • Output and input are not ohmically short circuited, it appears that the IC is operating normally but just never responding to any signal to not increase the output voltage. The switching behavior looks nominal to the best of my knowledge.
  • Replacing the IC with a spare had no noticeable affect.

Any ideas would be welcome - it's probably something simple, but so far this has eluded me.