This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25173: Leakage Question

Part Number: BQ25173


Hi,

The customer is using BQ25173 to charge the supercap.

With no voltage in the IN pin, a reverse current flows to OUT / FB / /PG / STAT Pin, resulting in leakage.(3.5㎂ at 3.6V)

CE : High, IN : 0V(VSUB not connected)

Is the consumption current of BQ25173 normal under conditions?

Please review if there is a problem with the customer's schematic.

If BQ25173 consumption current is normal, please recommend a product with a low consumption current.

GLBE : GCX10030

* R75 has a 0 ohm connection. *