Other Parts Discussed in Thread: TL432, LMV431, , ATL432

In the schematic diagram,(12V 5A), using the TL432, regulation is suitable up to 12V 2A; after that, the voltage drops significantly.
Replacing the TL432 with LMV431, the regulation is correct, with no more than a 3mv drop from 0 to 5A.
I need help with the circuit to work with TL432.
Thanks