Part Number: TPS7B7702-Q1
Other Parts Discussed in Thread: TPS7A8101, TPS7B7702
Hi Expert
For load regulation and line regulation:

test condition: VI = VO + 1.5 V to 40 V and VI ≥ 6 V, IO = 10mA, voltage variation on FB pin and result is 10mV
IO = 1 mA to 200 mA, voltage variation on FB pin and result is 20mV
but in TPS7a8101:

test condition: VOUT(NOM) + 0.5 V ≤ VIN ≤ 6.5 V, VIN ≥ 2.2 V IOUT = 100 mA, and result is 150 μV/V
100 mA ≤ IOUT ≤ 1 A and result is 2 μV/mA
Question: customer want to choose the device load regulation 1%(1mA~200mA) so I could like to calculate this value base on datasheet value.
Could you please tell me how to calculate this value base on datasheet form.