Hi,
My customer using MPS MP100L, if I want provide alternative part. Do you have better suggestion?
TPS7A78 seems only can provide up to 5V output voltage.
Thanks!
Jeff
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
My customer using MPS MP100L, if I want provide alternative part. Do you have better suggestion?
TPS7A78 seems only can provide up to 5V output voltage.
Thanks!
Jeff
Hello Jeff,
Competitor MP100L is an off-line regulator with an internal LDO that regulates 12V and supply 20mA. I would recommend TPS7A24 based on the information of the internal LDO and if supply voltage <18V. If the AC/DC regulator needed, then yes TPS7A78 is our only option.
Best,
Eunize Tobias