This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61372: Connect motor to output

Part Number: TPS61372

Hello,

I would like to ask you about the TPS61372.
Specifications are below.
I am assuming that a motor will be connected to VOUT, but are there any concerns?
Is it okay if the back electromotive force is applied to VOUT?

(Specification)
VIN: 2.5V to 5.5V
VOUT: 6V
IOUT: 600mA

Best regards,