Other Parts Discussed in Thread: GPCCHEM, BQ34Z100
Hi,
I'm trying to run a learning cycle for a 100Ah 12V AGM lead acid battery, and I cannot seem to get the Learned Status register to set to move from 0x04 to 0x05. I have attached the GPCCHEM report I got after a logged discharge (let me know if using chem 808 is appropriate, it may be too inaccurate), the log during the learning cycle and the gg file.
You may notice I have the design capacity in the fuel gauge set effectively to 75Ah (18750mAh * 4 scaling). This is because these batteries seem to only be giving me 75Ah on discharge to end voltage (this is an issue I'm discussing with the battery manufacturer). This said, I assume this shouldn't be an issue for the learning cycle.
Could I get some guidance on why this learning cycle is failing?
Thanks.
0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 Summary of all IDs with max. DOD deviation below 15% Chem ID max DOD error, % Max R deviation, ratio 808 4.23 0.19 800 4.85 0.17 809 6.7 0.24 804 10.33 0.74 810 12.32 0.6 802 12.83 1.19 812 13.04 0.51 813 13.58 0.52 801 14.92 0.83 Max. deviations for best ID is within recommended range. Chosen best chemical ID is suitable for programming the gauge. Selection of best generic ID for ROM based devices like bq274xx Device / Family #1 Generic Chem ID Device/ Voltage/ Chemistry max DOD error, % 128 bq27421-G1A: 4.2V LiCoO2 100 312 bq27421-G1B: 4.3V LiCoO2 100 354 bq27411-G1C: 4.35V LiCoO2 200 3142 bq27421-G1D: 4.4V LiCoO2 200 Best generic ID 128 Warning: Generic ID Deviation is so high that it is most likely due to anomaly in the data. Please check that data files have recomended format, units and test schedule Device / Family #2 Generic Chem ID Device/ Voltage/ Chemistry max DOD error, % 1210 bq27621: (ALT_CHEM1) 4.3V LiCoO2 100 354 bq27621: (ALT_CHEM2) 4.35V LiCoO2 200 1202 bq27621: (default) 4.2V LiCoO2 200 Best generic ID 1210 Warning: Generic ID Deviation is so high that it is most likely due to anomaly in the data. Please check that data files have recomended format, units and test schedule Device / Family #3 Generic Chem ID Device/ Voltage/ Chemistry max DOD error, % 3230 bq27426: (default) 4.35V LiCoO2 100 3142 bq27426: (ALT-CHEM2) 4.4V LiCoO2 200 1202 bq27426: (ALT_CHEM1) 4.2V LiCoO2 200 Best generic ID 3230 Warning: Generic ID Deviation is so high that it is most likely due to anomaly in the data. Please check that data files have recomended format, units and test schedule