Hallo all,
My name is Dennis.
I have a question about tps61200: i have a schematic with a supercap as power supply connected ti Vin of tps61200, supercap will be loaded up to 1,6-1,8V , C=100mF low ESR of about 10 Ohms. Would i be able to switch the tps on with a short Logic High Signal of about 5ms from a µC? If yes, would tps "go sleep" after 5ms and how much voltage at EN is requiered for such short on/off switch? The Purpose of the schematic is to switch with power from supercap an smd bistable relais (requieres power of 200mW at 5ms time).
Thanks