This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A02: Did TPS7A02 support 1.3V input and 1.2V output

Part Number: TPS7A02


Hi TI Teams,

Can u help to confrim that did TPS7A02 support 1.3V input and 1.2V output? If yes, how much conversion efficiency can be achieved at this time?

Thanks,

Kind Regards

  • Hi Lumina, 

    Our current fixed output options for this part are: 1, 1.2, 1.5, 1.75, 1.8, 1.85, 2, 2.2, 2.3, 2.5, 2.8, 3, 3.1, 3.3, 3.6V.

    However, depending on what load the LDO is support, the 100mV headroom may not be enough. 

    As for efficiency, this app note helps define efficiency parameters for LDOS https://www.ti.com/lit/an/slva079/slva079.pdf

    Using the figures on page 8, you can better calculate the efficiency of your application.

    but I can't estimate that without the load. 

    Best,

    Juliette